This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 温度采集返回的NTC阻值与实际的不相符

Part Number: BQ76952


我在用BQ76952的TS1、TS3、HDQ和CFETOFF脚连接NTC电阻时,设置它们的引脚功能为:18K上拉热敏测量模式、18K温度模式、热敏电阻温度测量,已报告但未用于保护 以及 ADC输入或热敏电阻。测试时室内温度约为25度,用万用表测量NTC电阻时阻值约为9.6K,但从BQ76952读回来的4路NTC的阻值都在300K左右,而通过子命令将上述4路NTC的ADC采集值读回来再换算成电压,结果都在0.63V左右,与实际结果相符。另外,上传的文件为我所用到的NTC电阻的阻值计算出来的系数,并将其对应的写入Calibration:180K Temperature Model各个RAM中,但读回来的阻值就是相差很大,是不是在采集NTC时,还有哪里需要注意的呢?bq76952-10K-NTCcoef-calulator.xlsx

  • 您好,请参考下面的帖子,跟您的问题类似。

    https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1003796/bq76942-accuracy-of-ntc/3719744?tisearch=e2e-sitesearch&keymatch=BQ76952%252520NTC#3719744

  • Star Xu,您好

    你发的帖子的情况跟我的是有一些类似,但那个帖子的温度值是相差几度,而我的是25度左右的检测出 -40度以下的温度,而且那个帖子最后解决的方法是Matt使用了一个内部了工具重新计算了一个温度系数来解决的,而这一工具又没有公布出来,请问你是否有Matt所使用的那一个工具呢?能否帮忙重新计算一个温度系数呢?

    谢谢

  • 问题已解决,BQ76952技术参考里面的关于NTC温度结果的单位写的是0.1K,是指开尔文温度,而我把它当成的阻值单位,所以计算有误。