This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ34202: 上电顺序控制

Part Number: LMZ34202


我想使用LMZ34202设计两个电源,输入均为12V,输出分别为3.3V和5V,且要求上电顺序为3.3V输出先于5V电源输出。查阅手册后,我用3.3V电源输出的PWRGD信号连接到5V电源的INH/UVLO引脚。

下面是我的原理图。

我觉得这样做理论上是可行的,但是PSpice仿真的结果显示5V电源始终没有输出,但3.3V电源PWRGD信号输出是正常的。

我想确认下我是否可以这样设计?谢谢。