This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1085: 过流测试时候,器件LM1085未关断(Shut down)和保护

Part Number: LM1085

在电源输入27V,输出24V测试时候:


1.在负载电流2A时候,正常输出24V电压,测试通过。

2.在过流负载6A时候,有一些LM1085零件不能关断或者有些稳压管几秒时间被击穿了。

   请问如何测试过流负载,仪器设备的纹波或者测试条件有什麽要求?

  • HI
         将你的测试电路放上来,或者说你是怎么测试?

  • 测试程序如下:

    1–测试空载电压:输入27V,输出24V.

    2–满负荷20秒,应能提供20秒的满负荷,不要测试更长时间,因为它将关闭。

    3–过载测试–这是为了检查调节器在过载时是否会关闭–我们确实遇到了一个问题,即IC出现故障,o/p电压与I/p电压相同–这是不好的。所以这个检查它是否关闭,测试规格说大于6A,我们已经看到需要8A才能使它关闭,所以不要将过载设置为6A,同样,这个测试应该不会持续很长时间。不要慢慢地加大电流,越快越好。

    4–恢复,因此停机后,卸下负载并再次检查o/p电压调节器。

    我们大概有20%的稳压管不能通过第三步的过载测试,即输入27V时候,输出没有关断。大概输出16V左右或者直接被击穿了。不知道是什麽原因?

  • Hi

        这个芯片的datasheet 关于过载描述非常不清楚,但是如果你加载到6A, 输出电压跌落严重就是保护了,并不一定要关断。之后芯片温度升高再热保护关断即可。

        你讲到的击穿是这个芯片击穿吗?