This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS57060-Q1: TPS57060QDGQRQ1的VREF在不同情况下的最小值、典型值和最大值

Part Number: TPS57060-Q1

请在以下条件下提供上述“VREF(电压参考)”的最小值、典型值和最大值:

Texas Instruments/ TPS57060QDGQRQ1

  1. VIN = 12V ~ 36V  ; TJ = - 40℃ ~ +85℃
  2. VIN = 23.5V ~ 24.5V ; TJ = +20℃ ~ +30