This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1843该怎么用

Other Parts Discussed in Thread: UC1843

UC1843该怎么用?最近在做一个太阳能充电器,输入25~36V,输出40~60V可调,现在只希望能做出一个可调占空比(0~100%或者0~50%),开关频率(100K~500K)(要求不高),的PWM产生电路,驱动5V的MOS实现电池的不同阶段的充电,在在线设计里面没办法选择输出可变,也找不到这方面的资料,希望能得到帮助。

  • 这个芯片有内部推荐图,可是输出可调?(属于什么意思),有机会回复我,我看看,如果要求输出功率一样的话,那是比较OK的,如果输出可调,只需要几个开关调档就可以了!