This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53659: TPS53659 PMBUS Programmer Script issue

Part Number: TPS53659

你好,

      目前有一个由Fusion Design Online工具生成的PMBUS Programmer Script。然后使用任意一个PMBUS 主控制器,播放PMBUS Programmer Script 包含的PMBUS数据包给TPS53659。

但是发现处理0x21命令时,写进器件寄存器的数据和读回的数据不一致。

PMBUS Programmer Script是这么规定的

Write VOUT_COMMAND [Rail #1] 1.000 V
WriteWord 0x21  0x9700
ReadWord  0x21  0x9700

Write VOUT_COMMAND [Rail #2] 0.900 V
WriteWord 0x21  0x8300
ReadWord  0x21  0x8300

但是实际用ReadWord 0x21读回的寄存器数据是0xBF, 0xCF,而不是写入的内容 0x97 ,0x83

问题1:请问这是什么原因呢?

问题2:在烧录过程中,是否可以忽略0x21命令的写错误?

谢谢!