Other Parts Discussed in Thread: TPS54260, LMR10510, TPS62290-Q1, TPS54260-Q1
各位大侠,正在做一个车载黑盒子的项目,能给推荐一下电源方案吗?
方案要求:
1. 车载应用,车用级芯片。
2. 电源9~60V输入(因为该黑盒子70%是用在汽车上12V供电,但是30%会用在一些特殊场合供电在40~50V左右),输出5V,3.3V,输出电流<1A。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS54260, LMR10510, TPS62290-Q1, TPS54260-Q1
各位大侠,正在做一个车载黑盒子的项目,能给推荐一下电源方案吗?
方案要求:
1. 车载应用,车用级芯片。
2. 电源9~60V输入(因为该黑盒子70%是用在汽车上12V供电,但是30%会用在一些特殊场合供电在40~50V左右),输出5V,3.3V,输出电流<1A。
Hi
9~60V转5V可以用TPS54260: http://www.ti.com.cn/product/cn/tps54260
5V转3.3V可以采用LMR10510: http://www.ti.com.cn/product/cn/lmr10510
汽车级的芯片,在芯片的后缀带有Q1的
电流小于1A的,可以使用TPS54160-Q1, TPS54162-Q1或者使用2.5A的 TPS54260-Q1 TPS54262-Q1
5V的锂电池是多少毫AH的??需要多大的充电电流??充电器也需要是车载级的芯片??
如果是的话,可参考:
Hi
如上汽车级别的应用,芯片选择需要带Q后缀的芯片。
转5V则需要用TPS54260-Q1, 5V转3.3V就需要选择TPS62290-Q1 .