This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

车载项目,能给推荐一下TI的电源方案吗?

Other Parts Discussed in Thread: TPS54260, LMR10510, TPS62290-Q1, TPS54260-Q1

各位大侠,正在做一个车载黑盒子的项目,能给推荐一下电源方案吗?

方案要求:
1. 车载应用,车用级芯片。

2. 电源9~60V输入(因为该黑盒子70%是用在汽车上12V供电,但是30%会用在一些特殊场合供电在40~50V左右),输出5V,3.3V,输出电流<1A。

3. 带充电电路,可以完成对5V的锂电池充电电池充电。
4. 可以实现主电源断电的情况下,锂电池自动供电
5. 在锂电供电情况下,可以通过MCU控制整机断电实现0功耗的待机功能
谢谢!