This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1117: 带载后输出电压降低,甚至直接没有输出

Part Number: LM1117


使用LM1117的ADJ版本,输入7V转5V  

反馈电阻设置1k和3k  输入电容10uF   输出电容100uF  使用datasheet推荐接法

更换反馈电阻1k和2.7k 输出电压是可调低的,空载下输出电压正常

空载下测试输出5V,但是此时上采样电阻两端的电压只有0.8V而不是VREF 1.25V,

输入7V一直是正常的

不太明白问题在哪里

带了10mA负载后,输出从5V掉到4.8V,再加10mA负载直接输出没了

之前使用中没遇到过这种问题,请问下该怎么改