This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25085: Dynamic load, inductive howling

Part Number: LM25085

VIN 24V,VOUT 12V,Imax:5A.The output voltage ripple is normal under static load, and there is no howling phenomenon; when 0.5A~3A dynamic load is executed, the inductor has obvious whistling.
When the RT is set to 100K, 200K, 200K, 300K, there is the phenomenon of inductive howling.I would like to ask how to remove the inductance whistling.