手册中表格2有12V输出的相关配置

6.3节中输出电压对应的SW时,输出最大28V;这里的SW模式是否是不连接Boot电容?
对于此芯片的一些疑惑请熟悉的朋友解答,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

手册中表格2有12V输出的相关配置

6.3节中输出电压对应的SW时,输出最大28V;这里的SW模式是否是不连接Boot电容?
对于此芯片的一些疑惑请熟悉的朋友解答,谢谢!
Hi
你给的2个表是不相关的,第一个表配置是12V输出的分压电阻阻值,cff,以及此时的电感感量,与输出电容。
而第二表是SW的耐压。
这个芯片是降压芯片,最大占空比是超过90%的, 也就是说你要输出12V,只要反馈电阻正确,输入电压超过12/90%=15V都是可以的。(实际上duty是大于90%,推荐按照90%来算,实际可能14V以上都是可以的)