This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR62421: 或LM3735做LCD背光驱动的问题

Part Number: LMR62421
Other Parts Discussed in Thread: TPS61500

要求5V输入,输出恒流530mA(电压10v)驱动LCD背光。这个芯片能不能实现。有没有输出过压保护功能?如果在LCD还未接入电路时电源相当于开路,反馈开路。会不会损坏芯片?

有么有其他合适的芯片可以推荐,谢谢。

  • Hi

        建议用LED driver芯片来做,大部分的这类芯片都是有开路OVP保护的。而类似LMR62421这类DC/DC的芯片基本上都是没有输出OVP保护的。

        例如TPS61500之类, 或者其他至少开关电流大于1.6A的LED driver芯片。