Part Number: TPS650330-Q1
在寻找可用的PMIC时,发现一款型号为TPS650320的芯片,与TPS650330只有两个PIN不同,TPS650330有I2C接口PIN,而320没有这两个PIN,330可以通过I2C进行配置输出不同的电压值,那么请问如何配置TPS650320的输出电压值呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS650330-Q1
在寻找可用的PMIC时,发现一款型号为TPS650320的芯片,与TPS650330只有两个PIN不同,TPS650330有I2C接口PIN,而320没有这两个PIN,330可以通过I2C进行配置输出不同的电压值,那么请问如何配置TPS650320的输出电压值呢?
Hi
我这边只能看到TPS65032Q1的评估板,没有找到其datasheet(或者是定制品之类,所以TI没有对外公布datasheet)
从评估板看是有I2C接口的,如果是这样就可以像一般PMIC一样程序控制。
如你所说,如果没有I2C接口,就像普通DC/DC一样固定配置输出。
所以在选择的时候要注意,如果你需要程序配置控制就选择TPS650330Q1, 而不需要或者没有程序置控制就选择TPS650320Q1.