This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27220: CEDV算法中,RSOC 在放电到7%以下时的估算机制

Part Number: BQ27220

你好:

       我们近期在对bq27220进行恒流(-100mA)放电(100%-0%)测试时发现,有的设备,RSOC从100%到7%正常(曲线平滑),但7%以下时曲线明显瑕疵,如下图,甚至还出现7%直接drop到4%的现象。

 请问:

1.7%以下时RSOC的估算机制是什么?也就是说,它是如何决定RSOC的值的,参考EDV和RawCoulombCount或者其它?请简单介绍下估算机制。

2.7%以上时的的RSOC的估算机制和7%以下时的估算机制是否相同,如果不同,请简单介绍下7%以上时RSOC的估算机制.

谢谢