This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331: audio noise found around the circuit

Part Number: TPS54331


Dear Sir,

I am using TPS51331 
input : 24V
output: 5V (~0.5A)

Using 22uH inductor with the typical circuit may found audio noise around the TPS51331 circuit.

Replace the inductor with a 6.8uH then no more strange audio noise. but the circuit will not be in the webench recommended range.

Will it a kind of danger to use the 22uH inductor?

  • HI

        已经在另一个帖子中回复:

        这个芯片是3A输出降压芯片,为了提升空载轻载的效率,芯片会出现 in pulse skipping Eco-mode 。在更大一点负载的情况下回出现第一个图的震荡现象,没有问题。通过调节电感会降低电感的峰值电流,对这种模式有一定的影响,波形会趋向正常。但是调了电感后也要调节补偿,环路不稳定可能导致电感啸叫。

        计算补偿很麻烦,你可以按照datasheet中设计案例的方式来计算。

        或者直接借助在线仿真webench得到电路, 这个时候只需要注意下你选择电容的ESR即可。