This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61200: 测得纹波23-25mV,噪声过大。

Part Number: TPS61200
Other Parts Discussed in Thread: LM2734,

之前使用LM2734的方案降压得到3.3V只有几毫伏的纹波,但是使用TPS61200纹波有22mV以上,使用电容滤波未见成效。

 PCB

  • Hi

        datasheet或者EVM板上参考设计虽然没有给出重载下的输出电压波形,但是datasheet 第17页给了轻载的纹波,远大于22mV(大约40mV左右),一般重载下纹波会小一些,20mV多是正常的,有些芯片设计的比较好十几个mV也是有的。(而且TPS61200是boost, LM2734是buck芯片)

        如果你希望纹波尽量小一些,在原有的输出2个10uF后面增加一个磁珠加10uF电容构成CLC, 应该可以做到效果很好的(TI有案例,纹波做到了5mV以内)