This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23758: 请教下各位,设计的板子反激隔离式POE芯片TPS23758的24脚波形有明显的上过冲现象,变压器二次侧输出有明显下过冲,带2A负载的时电压输出电压被拉低到3.9V了,电路是参考TPS23758EVM开发板设计的,变压器是找厂家参考LDT1018-50R定做的

Part Number: TPS23758

请教下各位,设计的板子反激隔离式POE芯片TPS23758的24脚波形有明显的上过冲现象,变压器二次侧输出有明显下过冲,带2A负载的时电压输出电压被拉低到3.9V了,轻载时候是5V,电路是参考TPS23758EVM开发板设计的,变压器是找厂家参考LDT1018-50R定做的,TPS23758工作在抖频模式下,无论带不带负载,都有上下冲现象

测过TI的demo板TPS23758EVM没有过冲和上冲,请各位帮忙分析下导致上下冲原因和带负载满足不了输出电压被拉低到3.9V的原因;

这个是原理图

 

这个图是TPS23758的24脚的波形,很明显有8V的上冲

这个是是输出变压器二次侧脚输出的波形,下冲有3V多;

下图是下冲波形部分

这个是上冲的波形细节,有五六个高频谐波,频率大概50Mhz