This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24168: BQ24178过温保护设计

Part Number: BQ24168


您好!根据BQ24168的规格书设计的电池过温充电保护电路,做了实验发现电池表面在达到设定值(45°C)之后,还是能继续充电,想让你帮忙看一下我们的电阻值是否计算正确

我们使用的电池里面带的NTC热敏电阻阻值为10K,其温度对应的阻值请看NTC阻值对应。

我们设定电池充电温度为0°C-45°C,根据芯片上的公式以及NTC阻值对应表计算得R29约为9.8KR30约为31K,实际板上应用的R2910KR3033K。经过实验发现,做了实验发现电池表面在超过45°C之后还是能充电,麻烦看一下我们的计算结果是否正确,如果不正确,请帮忙指出改善,谢谢。