Part Number: LM3481
Hi Team,
想了解LM3481在不同的输出电压下对应的输出电流是多少。
比如500V电压最大电流是多少?300V最大电流是多少?60V最大电流是多少 24V最大电流是多少?怎么计算出来的。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM3481
Hi Team,
想了解LM3481在不同的输出电压下对应的输出电流是多少。
比如500V电压最大电流是多少?300V最大电流是多少?60V最大电流是多少 24V最大电流是多少?怎么计算出来的。
谢谢!
Hi
这个没有办法评估的,一般DC/DC,类似LM3481的一般设计就几十瓦,但是同时电流也不会做的很大(5A左右),所以我一般这样判定,如果输出12V,可能设置最大5A, 但是如果300V,可能就200mA甚至更小,同时考虑额外增加驱动。