在测试LM5007低温-40环境下,输出比常温下高0.5V, 反馈电阻采用两个1K 1%电阻,1)麻烦问一下在低温环境下LM5007的内部电压基准会有改变吗?2)输出升高的原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
虽然这个datasheet中没有提供反馈基准在全温度下的变化曲线,但是即便在恶劣不会超过反馈的基准的tolerance范围2%,而你这里有10%。能够提供这个时候的输出电压波形? 这里的偏高可能是输出不稳定引起的。
请问你输出反馈纹波取样是采用什么样的方式,看看是否是这个的影响?串联电阻的方式应该温度影响最小(或采用ESR较大的输出电容),其它2种影响应该相对大一点。