Part Number: TPS61030

这是原理图,输入VCC为电池电压(2.7-4.2V),输出为5V。按目前设计BAT_VCC端接上5Ω负载,输出电压会被拉低。现电路带载最大只能带1.2A,而且输入端电压会被拉低0.3V(用的直流电源测试,直流电源设定为3.5V,到VCC端实际上只有3.2V)。电感SWPA6045S6R8MT(顺络电感)饱和电流为3A。
我想设计的电路带载能力最好能达到2A,且不会把5V电压拉低。请问下该如何修改??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS61030

这是原理图,输入VCC为电池电压(2.7-4.2V),输出为5V。按目前设计BAT_VCC端接上5Ω负载,输出电压会被拉低。现电路带载最大只能带1.2A,而且输入端电压会被拉低0.3V(用的直流电源测试,直流电源设定为3.5V,到VCC端实际上只有3.2V)。电感SWPA6045S6R8MT(顺络电感)饱和电流为3A。
我想设计的电路带载能力最好能达到2A,且不会把5V电压拉低。请问下该如何修改??
HI
电路上看没有看到输入电容,建议增加10uF~22uF,尽量靠近电感输入端。
需要达到2A负载,建议电感饱和电流选择4.5A. 按照你的设计,输出10W, 效率90%, 输入2.7V时,此时输入电流为4A, 峰值电流大约4.8A, 早就超过3.6A的保护点,所以负载到不了2A.
如果要输入2A, 建议输入电压需要做高一些,10/0.9/(3.6/1.2)=3.7V.