This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51501-Q1: 工作异常,问题紧急处理!重要!!!

Part Number: LM51501-Q1


电压输入12V快速降低到3V,发现BOOST无法启动,经查发现电压输入12V快速降低到3V过程中,VIN会被拉低到约0.2V,而我们的Vin是接到使能脚的,并且我们LM51501的VIN的输入电压下限也是1.5V,所以这个时候BOOST无法工作。想了解为什么VIN会被拉低到0.2V。无论是降低电压到3V还是3V恢复到12V都有这种情况发生。从status脚可以看出BOOST是工作了一段时间的。图片不知道怎么放上来,可以联系我的邮箱,谢谢。