This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25200: OCP电流须维持多久TPS25200才会启动保护

Part Number: TPS25200


TPS25200 可利用RiLim  设定 Current Limit , 可当做过电流保护(over current protect)
RiLim 用80.6K , Current Limit 范围是1110mA - 1300mA
请问
1. 当电流为1110mA-1300mA时 , 电流须维持多久TPS25200才会启动保护
2. 当电流是1110mA时启动保护,电流下降到1110mA的多少百分比时,TPS25200才会关闭保护呢?
   1110mA 的-1%还是-2% 呢?