1. 极轻载时,输出纹波会有较大高频尖波,放大可以看到明显跌落;如图2/图3;
2. 5%-95%大动态负载时,输出电压偶尔出现较大跌落,从初级驱动来看,问题在于负载切换刚好落在burst模式的间歇时间内,请问是否有解决办法?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 极轻载时,输出纹波会有较大高频尖波,放大可以看到明显跌落;如图2/图3;
2. 5%-95%大动态负载时,输出电压偶尔出现较大跌落,从初级驱动来看,问题在于负载切换刚好落在burst模式的间歇时间内,请问是否有解决办法?
已经有增加过2倍了哦,(330uF→330uF*3),可以适当缓解电压跌落幅度,但是没法彻底解决。
Hi
如增加输出电容,仅仅有改善,就需要确认反馈。
反馈部分,主要需要调节哪方面呢?
增益裕量还是相位裕量,或者穿越频率?
Hi
将电路贴上来看一下,一般可能是”异常“影响了反馈的速度。
电路图如上,谐振参数:Lr=75uH Lm=520uH Cr=30nF n=26:7 额定满载54V/2.76A
HI
对照: https://www.ti.com.cn/cn/lit/ug/sluubx3b/sluubx3b.pdf 调整一下431补偿和光耦电路(CF1)看看
感谢您的答复;
问题已解决(IC在极轻载若不进burst mode容易误触发ZCS保护,导致工作紊乱;ps:样机burst阈值调到了最低)