This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131: 输出电压精度?

Part Number: TPS65131

请问TPS65131 的电压输出精度是多少?我在设计的电路里,用了-15V,实际输出到-16.2左右,这正常吗?

  • 产品的数据表里没看到这个参数

  • Hi

        反馈基准精度1%, 反馈电阻精度1%,输出总的精度不超过+/-3%, 或者见datasheet 参数表第五页Total Output DC accuracy  3%.

        -16.2V肯定是超出范围的,首先建议你确认选择的反馈电阻,及精度。 如果没有问题,测试一下波形看下,看是否是纹波或者noise比较大导致的,如果是你就要确认layout(反馈受到干扰),以及反馈的GND(建议选择模拟GND)