最近想自己做个12v,9000mah的锂电池组,想用6节4.2v 4500mah的锂电池2并联3串联达到12v,9000mah,但是由于锂电池不能过冲过放,所以就想给锂电池做个过冲过放的保护电路,网上大致查了下,很多ic都支持3-4节单个锂电池串联起来使用,对其保护,我的疑惑是:我的2并3串电池组,能否将2并的电池看成是一个锂电池,这样3串电池组就刚好相当于3个锂电池,再按对应ic上提供的接法接入电路进行保护呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我还有一个疑问就是:这样锂电池先2个一并组成一组,再3组串成一个12.6v,9000mah的电池,这其中有个问题就是,如果那2个一并组成的电池组里面有一节电池是3v,而另外一节是4v,这样并联后电池组每节电池电压会大概都是3.5v左右,这样给他们充电时,会不会出现冲到4.3v时,这组电池就不被充电了,(被保护ic保护了)但是此时单独测这组的2节电池电压,一节会是4.3v,一节还只有4v,这样不就有一节电池没充满电吗?我需要的是2节都充满电啊。Lewis 说:当然可以。笔记本的电池都是这样做的,你可以直接选择现在的笔记本电池管理芯片BQ3060,BQ3050等,即可以实现保护功能,还可以计算电量。