This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62110: 希望能帮忙解答TPS62110的一点问题

Part Number: TPS62110


希望能帮忙解答TPS62110的一点问题,现在有一个低输入电压的情况,我看datasheet上面说最低输入电压为3.1V,那在应用于VIN=3.1V时是否有很大概率触发欠压锁定?芯片是否很不稳定?

我看datasheet电气特性表上面说在在VIN≥3V时输出电流典型值为100mA,但是在典型特性仿真图里面看VIN=3.1V时输出电流几乎为0。

 

  • Hi
        这个芯片最低输入电压3.1V, 和其他芯片欠压保护UVP不同,它的欠压保护最高点就定义在3.1V, 典型值在3V,  也就是说低于3.1V都可能欠压保护,那么在应用中输入存在纹波或者瞬态的略微拉低是有可能造成欠压保护的(很多芯片最低输入电压和欠压保护电压之间一般都是有零点几伏的buffer的),所以这个建议实际操作中输入电压最好大于3.2V,保留0.1V的buffer,当然略微再放大一点点更好。