This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24196: BQ24196的Ilim设置

Part Number: BQ24196

我设计的充电电流是2A,如果将Ilim设置成2.5A,插入到比如台式机电脑的usb中,会不会导致电脑的usb口被拉死的情况出现?

但我如果将Ilim调低,又限制了充电电流,是不是我哪里理解有误,帮忙解答下,感谢!

  • Hi

       这个你要确认用的USB接口最大输出电流,如果最大电流只是1A, 是会被电压拉低的。 BQ24196最大充电电流要依据输入功率来设计。

       例如假设你输入5V最大1A, 充电效率80%, 最大充电功率就只能是4W,  然后再结合充电电压和电流来估算最大充电电流。