Other Parts Discussed in Thread: LP3906
使用LP3906SQJXXI,只使用DC/DC两个通道(3.3V和1.2V),实测3.3V通道工作电流为162mA,1.2V通道工作电流为123mA。输入5V电流有231mA。计算可知转换效率只有60%。距离手册所描述的95%和85%(查手册的效率曲线)很大。
望高手指点!!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LP3906
使用LP3906SQJXXI,只使用DC/DC两个通道(3.3V和1.2V),实测3.3V通道工作电流为162mA,1.2V通道工作电流为123mA。输入5V电流有231mA。计算可知转换效率只有60%。距离手册所描述的95%和85%(查手册的效率曲线)很大。
望高手指点!!!!
Hi
如果仅仅是两路DC/DC 效率只有60%, 还建议检查如下:
1. layout上Vin1/Vin2的10uF电容尽量靠近芯片。
2. 电感选择尽量低的DCR.
就DC/DC而言,如果每一路DC/DC的效率在90%左右,总的效率也应该在90%左右,可以手测一下芯片是否很烫,如果不烫,很可能是电感的质量问题。
Hi
用示波器测试一下Vin脚的电压是否存在较大的纹波,如果是稳定的输入,计算效率时此Vin脚电压为准。否则需要在Vin处焊接电容到GDN(可选取一路), 然后输入电压直接给到Vin 脚(也就是说不要过孔走电流), 然后实测Vin脚电压算效率。因为你的layout输入电容在背面,并走孔到正面可能存在影响。
电感选择DO3314-222MLB, DCR是200mohm, datasheet推荐的电感规格中DCR是70mohm,所以可以优化,但这不是造成效率偏低的原因。