This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2897A: 有源钳位UCC2897ARGPR 做电源砖无输出电压

Part Number: UCC2897A


1,设计参数:

UCC2897A 用于有源钳位正激时,设计相关参数如下:

输入:VIN=54V 

输出:VOUT=12V/10A 

变压器占比:初级NP次级NS:辅助绕组Nr=8:6:5,感量200uH

2,问题描述:

1)使用直流电源13V/0.5A单独给UCC2897A的VDD供电是,VDD会把直流电源13V/0.5A拉低到比较低的电压值,

2)实测UCC2897ARGPR  芯片的VIN(pin18)引脚和VDD(pin)之间的阻抗只有61Ω,测试新的芯片阻抗也是61Ω,这个阻抗是否正常?

3,待解决问题:

1)帮忙排查下原理图设计是否有问题

2)针对无输出电压问题,请提供一些建议和思路。