This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2553D: TPS2553D 能否作为电池充电用的 负载开关?

Part Number: TPS2553D
Other Parts Discussed in Thread: TPS22929D, TPS22918, TPS2553

你好! 

      我司使用 TPS2553D 作为聚合物锂电池充电用的负载开关,锂电池的容量是2600mAH, 输入电压为5.4V,电池最大充电电流为1.3A。

      我们把 限流电阻 RILIM 设置为15KΩ,此时限流1.7A。

     但是部分电池充电时会出现指示灯红蓝闪烁问题(即充不进电),测试充电电流周期性有7A的电流脉冲导致指示灯一直红蓝闪烁。

      但我们把IC 更换成 TI 的 TPS22918(2A) 或者 TPS22929D (1.8A) 充电时, 能充进电,指示灯不会红蓝闪烁。

      问题: 1. TPS2553D 能否做为电池的充电负载开关? 还是只能用于USB的电压供电? 

               2. 为什么充电时会出现7A 的大电流脉冲输出,什么原因导致的?

      Thank you!