This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63802: PS63820

Part Number: TPS63802


mode引脚接地,使用低功耗模式,反馈电阻选择511K和91K,精度1%,输出3.3V,在使用中负载功耗从100uA突然提高到150mA时,电压有3.35V降到3.33V,压降0.02V, 150mA持续时,开关电源输出的电压一直保持在3.33v,是否调整反馈电阻的精度提高到0.1%,开关电源会通过调节开关频率将3.33V提高至3.35,或者有别方式防止电压降低后能够快速提升(不适用PWM模式,太耗电)

  • Hi

        首先需要说明是一般开关电源输出电压的范围精度是+/-5%,  而反馈电阻的精度是1%,反馈基准的精度是1%, 所以实际输出电压的控制精度在3%以内(最差3%,实际1%~2%内), 所以输出3.3V的精度是3.3V+/-3%以内都是可以的。

         而空载下3.35V, 带载150mA后输出电压略微降低,并非反馈电阻精度的原因,而是因为反馈环路的原因,在负载增加下,电压略微降低是正常的。