Part Number: TLV767-Q1
Other Parts Discussed in Thread: INA280-Q1, TLV767
我的设计需求是Iout=
0.8A,那么我在数据手册上看到的设计过程,没有关于Iout的;Iout取决于负载的话,按照我这样的接法给INA280-Q1电流采样芯片供电,能提供0.8A的电流吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TLV767_Q1是1A LDO ,所以输出最大1A没有问题(0.8A也没有问题), 但是你需要注意,LDO一般要避免高功耗,特别是输出电流较大的LDO, 如果输出0.8A, 输出输出之间的压差不能太大,例如假设压差是2.5V, 这样LDO功耗就是2W, 芯片的温升可能就是110℃左右,加上环境温度,很容易就超过芯片推荐温度范围125℃。
所以要输出0.8A, 要么尽量减小输入输出压差(选择尽量低的输入电压源减小压差或者前面增加DC/DC), 或者尽量降低LDO的热阻。