This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 上电初始化问题

Part Number: BQ76952


我们设计了一款BMS板子,在上电复位之后,有时候初始化成功,有时候初始化不成功。

如果初始化成功的话,会产生alert信号,可以正常读写BQ76952寄存器已经进行设置。

不成功的话,通过MCU的单步跟踪调试,发现发送BQ76952地址0x10之后无ACK返回。

复位信号由MCU GPIO 产生100ms的高电平,连接到BQ76952的RST_SHUT引脚。

请问上电初始化或者复位之后应该怎样对BQ76952进行操作设置?