Other Parts Discussed in Thread: BQ25070, BQ24172
用bq25070给单节3000mAh LiFePO4电池充电,充电电流默认285mA(将CTRL直接接地),用285mA电流充电,时间太长。
所以用1A充电比较合适,设置1A的充电电流需要发11个50us以上的脉冲信号到CTRL端。
是否可以不用单片机而让bq25070默认把充电电流设置在1A? (因为单片机会增加体积和成本)有没有更简单的电路实现默认1A电流充电。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Udsong Lu,
你好,25070 的确需要使用脉冲信号来进行充电电流的配置。且其默认的充电电流目前不能设置在1A。
您可以考虑使用bq24172,这款芯片可以调整充电电压来满足LiFePO4的充电要求