This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65261-1: 低温环路不稳定,如何快速修改验证

Part Number: TPS65261-1
Other Parts Discussed in Thread: TPS65261

        我司HR650中转台项目使用TPS65261-1为TMS320C4748 DSP供电,低温下发现环路不稳定(-10℃以下有问题,-10℃以上没有问题),输出电压异常,机器无法开机. 如下分别是不同温度测试的环路曲线(3V3D 空载)及原理图使用的补偿参数,帮忙看下如何调整参数,保证低温下环路稳定.  测试的波形主要是3V3D,我们怀疑1V8D和1V3D也存在相同的问题,因为-40℃下有测量到SW开关抖动严重(常温下没有),抖动有超过占空比的20%. (3V3D早期环路电阻R2031是15K,发现无法正常拉负载,100mA就没输出了,后来改到8.2K,可以正常带负载)

3V3D空载不同温度下环路曲线及1V8D低温SW开关波形.docxTPS65261-1PMU参考电路图.pdf

TPS65261-1PMU参考电路图.pdf

3V3D空载不同温度下环路曲线及1V8D低温SW开关波形.docx