Other Parts Discussed in Thread: SN65HVD1781,
电路设计使用了参考电路。只输出+5V。
输出端电容0.1uf,输出端0.1uf和10uf。然后Vrec连接10K电阻之后到ENABLE 然后接了2u2的电容到-Vout。
给三个SN65HVD1781做隔离供电。其中只有一个RS485和外部连接,只有A,B两个线连接到总线,未连接地。其他两个RS485没有对外连接。
当RS485总线上其他节点已经上电的情况下。且其他节点在周期发送数据时,给本节点上电,此时发现有时DCR010505的输出为0.
当给总线上接上一个USB转RS485后,同样上场景下,不再复现。
或者DCR010505的输出为0后,此时给RS485总线上接上一个USB转RS485后。DCR010505的输出可以恢复。
目前还没有测试这种热拔插时,DCR010505的输出电流。
问题:
1.是否因为热拔插造成冲击电流,导致DCR010505过载?
2.如果输出过载,是否DCR010505就会一直输出为0?