按照参考原理图,接两串电池,STAT引脚灯一直闪烁,OVPSET引脚电压实测1.06V,请问是什么原因呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
OVP保护点是1.6V,确认一下其他保护, 见datasheet 第24页table3.
Hi
OVPSET只是个分压,在0.5-1.6V范围内;用示波器测量,发现AVCC好像存在问题,移除电源和电池后,AVCC引脚会慢慢放电,上电时序与PAGE12不一样...

另外,SW引脚电压是0.85V左右,电池电压7.5V,TS电压2.8V(3.3x30.1/(5.23+30.1))
Hi
TS电压异常,datasheet TS电压应该在T1~T5范围内。