FB上下限为0.596±2.5%,但是BOOT脚输出超过上限7V,MAX值在7.2V。是否有问题。
另外想问下测试BOOT的引脚电压应力,用什么测试方法呢。
目前用以下方法:
1.使用Tek的3系示波器,探头采用Tek的地环线;
2.示波器全带宽,采样模式设置为峰值采集。
3.测量值读取示波器上的max值,是否ok.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.