TPS5430输出波形不正常,PH端有杂波导致最后输出成了锯齿波,而不是直线。我用的输出电感是4.7uH,输出电解电容是470uF/25v.
VIN输入范围是18V-30V,要求输出16.8V的电压和600mA的电流。
求高手解决。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于你的问题,这里有两个部分供你参考
1:如果按照你给的应用输入电压 输出电压和最大输出电流值等这些条件,4.7uh电感是满足不了你设计的buck电路进入ccm模式的最小要求的,建议你根据datasheet中的电感选择合适的电感-100uH。
2:如果按照最低18v的输入电压,此时的占空比已经超出了 TPS5430的最大占空比要求,所以无法进入稳态,所以要使用TPS5430这个器件必须要保证小于器件的最大占空比限制,如果18V的输入电压必须要保证,则建议你选择占空比更大的Buck dc-dc转换器。