如果按照最小VIN=VOUT+VDO计算,VIN=1.2V(VFB)+0.15V(VDO最大值)=1.35V,而不是规格书中说的1.7V,这是为什么呢?
If the minimum VIN=VOUT+VDO is calculated, VIN=1.2V(VFB)+0.15V(maximum VDO)=1.35V, not 1.7V as stated in the specification, why is this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
芯片输入最低电压1.7V是必须遵循的,Vin> Vout+Vdrop是LDO正常工作必须遵循的,两者都要。
所以在此情况下,输入电压必须大于1.7V.