This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63802: TPS63802用于TEC电路的问题

Part Number: TPS63802

您好,我用TPS63802做了一个TEC电路,电路是仿照你们给的MSP430方案设计的,只是把MSP430换成了STM32,但是出现了如下问题:刚开始只焊接了TPS63802以及能保证其正常工作的外围电路,FB反馈电阻511K和91K,输出电容22uf*2,输入电容:47uf钽电容*1+22uf*1+10uf*1,测得输出3.3V,正常工作。但是在焊完剩下的电路之后,上电测试输出电压只有0.25V,单片机没有烧写程序。然后我把单片机和TPS63802相连接的地方全部断开,输出电压仍然是0.25V,我还测了PG和FB的电压,分别是0V和0.09V。整个测试过程我给TPS63802和单片机加的输入电压都是3.3V,是通过5V适配器和AMS1117获得的。

我想问的是,这种情况是TPS63802损坏了吗?如果要实现这个TEC电路,有哪些好的建议呢?