看芯片资料最大可以达到400mA,但是里面推荐的电路图中都只有十几mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
400mA是典型的开关限制电流,并非最大输出电流。对于升压芯片,假设效率是85%, 最大输出电流Vo*输出电压/效率= 最大输入电流*输入电压。 而1.2倍的最大输入电流需要小于350mA(最小电流限制),同时还建议留有一定余量。
HI
达不到,但是十分接近,建议如果最大负载180mA, 可以选用(需要留一些裕量,避免过载)。