tps54295是双通道的电压转换,如果要求一通道输出正,一通道输出负电压,这对于芯片的地连接有什么需要注意的,这种正负输出可以实现吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
qiaoling ge 说:tps54295是双通道的电压转换,如果要求一通道输出正,一通道输出负电压,这对于芯片的地连接有什么需要注意的,这种正负输出可以实现吗?
请参考E2E上面的回复:
原帖地址:
http://e2e.ti.com/support/power_management/non-isolated_dcdc/f/196/p/262752/918948.aspx#918948
I think that is not possible as the grounds are common. I would recommend this approach:
qiaoling ge 说:相类似于这种的设计应用在tps54295,能实现两边正负同时输出吗?我是想到时候可以调节反馈电阻然后可以再另外调节电压的,谢谢啦!
你的反馈电压FB2是负值,我不认为TPS54295可以实现环路控制。
而提供的那个解决方案,输出的地是浮地,反馈电压还是是0.8V。