TI E2E 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55288: TPS55288RPMR

Part Number: TPS55288

使用外部输出电压反馈

1,输入电压为24V,设计Vout为12V,实际无输出,示波器抓取上下管波形,无驱动波形输出。

2,规格书上面Vref:45mv~1.2v,使用外部输出电压反馈,实际Vref取值多少呢?

  • Hi

       1.  如果启动测试完全没有驱动输出,你需要首先确认电路(芯片)焊接,如果没有问题,在确认一下EN脚,以及VCC脚电压是否正常?

       2.  见datasheet 第7页参数表 VREF