This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54040: TPS54040DGQR问题咨询

Part Number: TPS54040

你好,

   1、我们在家用控制器产品中使用TPS54040DGQR时出现一些问题,电路图如下:输入12V,输出10.8V。还有其它信息是:①不良品上电时,C1的电压是2.2V左右;②逐渐增大输入电压,C1电压也会慢慢上升;当输入电压增大到13.8V时,C1电压有个跳变升高(具体值忘记了),输出电压10.8V正常;然后把输入电压降到12V,输出电压维持10.8V不变。

   2、经与初步分析;TPS54040DGQR 芯片输入电压12V,10脚工作电压10.8V,实测不良品板子芯片10脚输出电压9.42V,芯片未能完全工作。

      确认1:取测试NG的不良品4PCS,将TPS54040芯片与测试OK4PCS良品的TPS54040芯片对调后,不良故障跟随芯片(即不良产品更换良品产品的芯片后,不良品再次测试OK,而良品产品更换成不良品芯片后,再次测试产品NG

      确认2 : 给不良品芯片10脚增加30MA的假负载后,测试5台,有4台产品芯片能正常工作。

请问一下,这是什么原因导致的呢?