Part Number: TPS2121
负载电流评估不足,实际最大值可能是5A,大于芯片最大限流设计值(4.5A)。
IN1和IN2同时存在,按照手册的表格Output Source Selection Table,MODE选的是VREF,OUT是IN1。
能否在不去掉TPS2121的情况下,不用TPS2121的切换功能,把IN1与OUT直接短接?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS2121
负载电流评估不足,实际最大值可能是5A,大于芯片最大限流设计值(4.5A)。
IN1和IN2同时存在,按照手册的表格Output Source Selection Table,MODE选的是VREF,OUT是IN1。
能否在不去掉TPS2121的情况下,不用TPS2121的切换功能,把IN1与OUT直接短接?
Hi
也就是相当于2路并联使用,但是输入源并不具备均流,所以不能这样用。
并且你IN和OUT短路,就是不用这一路控制,所以实际用一个短路开关控制应该也是可以的。
IN1和IN2是同一个电源出来的,原本设计默认用IN2,电流比较大的情况下需要外接一个电源也就是IN1,多一根线。
当前是板子已经设计好了,在不改板的情况下,短路开关控制不合适,似乎也没有同封装限流值更大的器件可以替代。
我的意思是IN1和IN2是同一个电源网络,物理上是导通的。另外手册里Feature标注限流4.5A,但是在Electrical Characteristics中RILM = 18.7kΩ时,限流的典型值是5.2A,我是不是可以把限流改成5.2A就能解决这个问题了?