Part Number: BQ25723
请教问题:我利用EVM的电路设计了电池充电电路,当用适配器供电拔下适配器切换电池供电的时候会有大于500ms的一个掉电过程,因为我的设备要求没有电池的时候适配器可以供电使用,因此我的电源切换电路是用MOS管在电池的外面搭建的。我想咨询一下是我寄存器设置的问题,还是电路上的问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ25723
请教问题:我利用EVM的电路设计了电池充电电路,当用适配器供电拔下适配器切换电池供电的时候会有大于500ms的一个掉电过程,因为我的设备要求没有电池的时候适配器可以供电使用,因此我的电源切换电路是用MOS管在电池的外面搭建的。我想咨询一下是我寄存器设置的问题,还是电路上的问题。
这个是我外部加的电源切换电路,请看一下是否是因为MOS管的切换导致的延迟,还是因为我的配置问题。充电配置参数有什么特别注意事项。我的电池是18650芯,两并四串。
您好,如果 Vin 降至 3.25V 阈值以下,转换器会重启上电序列,至少有 200ms 的延迟。
了解了。还有一个问题想请教一下,就是电池充电的时候需要每次I2C通讯控制,还是只设置一次后面就不用设置。如果是每次设置我这边是不是充电的时候需要CPU工作才行。如果去掉电池单独充电怎样操作。或着说有更好的电源管理方案也可以推荐。
当 Vin 或 VBAT 高于 3.25V 时,I2C 通信运行。 无法在没有电源的情况下启动通信。