This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3150: 瞬时电流输出能力

Part Number: LM3150

测试条件,LM3150输出电压给LED的阳极,LED的电流需求为4A,LED的调制频率为6MHz,调制频率在LED的阴极进行开关控制,

在低端的电流监控电阻上测到的调制信号,正常来说应该是方波,但是,实际测出为锯齿波,只有峰值处达到了4A的电流值。但是阳极的供电电压并没有被明显拉低(降低0.1V)

问题,是否LM3150的瞬时电流输出能力不足?

  • HI

         LM3150是外部MOS控制器,本身负载能力可以做到很大的,如果怀疑带4A异常,你可以用电子负载确认一下是否电路异常导致实际带载能力下降?

         或者直接用外部电源供应器来验证是否是电源问题。