输入电压:6-12v 输出电压:12V 输出电流 2A以上 有满足的DCDC电源芯片吗
应用场景:平时用7.4V锂电池供电,最低降到6.4V关机。但有时会用12V适配器给电池充电,充电过程中,用12V适配器给设备供电。
因此输入电压范围较广。要做到电池供电和适配器供电完美切换。
对电源波纹要求不大,最好外围电路简单点,希望能提供一款合适的芯片。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
可以选择LM3481/LM3478之类外部MOS的控制芯片
或者选择内置MOS的TPS55340之类
或者你借助在线仿真webench选型,从上述芯片界面的webench 进入,然后点击“new design”可以显示更多的方案,然后再按照你的要求在方案中筛选。